Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

An alliance for the IIoT

Companies are working on an open ecosystem for the digital transformation of industrial plants

Fecha de publicación: 02.04.2019

Founding members of the alliance are Beckhoff, Endress+Hauser, Hilscher, ifm, KUKA, Multivac and SAP. In principle, the alliance is open to all companies. Balluff, Gebhardt, Pepperl+Fuchs, Schmidtsche Schack, Samson and WIKA have already joined the alliance as members. All companies are mutually committed to the creation of a standardized and open ecosystem for the operation of highly automated factories and process plants with the integration of logistics and services.

“The open architecture of the Open Industry 4.0 Alliance meets all the requirements of the process industry,” emphasized Matthias Altendorf, CEO of the Endress+Hauser Group. “It is based on standards, ensures transparency across all business processes and guarantees the integrity of the systems. This enables process plant operators to leverage the potential of digitalization.”

Focus on implementability and benefits

The alliance members are planning to realize a so-called Open Industry 4.0 Framework based on existing standards such as I/O Link, OPC UA and RAMI for the entire route from objects in the workshop to services. Customers can choose from a modular system of compatible and scalable solution and service components, such as digital services from Endress+Hauser’s Netilion IIoT ecosystem.

The connection to the SAP software portfolio ensures the integration of a company’s business processes as well as collaboration with partners across company boundaries. The open architecture allows the simple connection of further system landscapes.

More information about the Open Industry 4.0 Alliance will soon be published at www.openindustry4.com

More information on Endress+Hauser’s digital services is available at www.netilion.endress.com

Visit Endress+Hauser at Hannover Messe 2019, hall 11, booth C43!

Descargas

    EH_2018-04-02_IO4_Alliance.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto